Convergent mode sensor
Pepperl+Fuchs expands its series 31 photoelectric sensors
Pepperl+Fuchs RL31-8-HGU-300-RT convergent mode sensor with fixed cable or M12 connection
Pepperl+Fuchs has expanded its tried-and-tested range of Series 31 photoelectric sensors with a new convergent mode sensor. This is available from Pepperl+Fuchs, both with fixed cable and an M12 connection.
You can use the new RL31-8-HGU-300-RT convergent mode sensor in the storage and conveyor industry. The new convergent mode feature helps to avoid faulty switching from incorrectly reflected light from objects that are located behind the actual target object. This means that reflective objects moving in the background are no longer a source of interference for your application.
Features of the new 31 series convergent mode sensor:
- Suppresses backgrounds with interference sources
- Easily visible LED display
- High-performance 4-in-1™ output
- Red light emission
- Compact and stable housing
- Protection degree II