Pepperl+Fuchs presented a wide range of new products at the SPS/IPC/Drives 2007 event.
In this issue of our e-news publication, we'll review highlights of the show.
Your Pepperl+Fuchs e-news Team
Up-to-date
VMT Bildverarbeitungssysteme GmbH moves company headquarters to Mannheim More room for new ideas
VMT Bildverarbeitungssysteme GmbH moved on 1st October 2007 from Weinheim to Mannheim, Germany. The company outgrew its former location due to an increase in personnel, and activities following integration into the Pepperl+Fuchs group.
Inductive reduction factor 1 sensor with increased sensing distance NRB: 12 mm semi flush with 18 mm housing diameter
With NRB12, the new member of the family of reduction factor 1 sensors from Pepperl+Fuchs, the optimal coupling setting between sender and receiver coil guarantees highest sensing distances and material-independent detection of all metals. The main component of the new reduction factor 1 sensor NRB12 is the print-coil system, which is comprised of a sender coil and a receiver coil. The downstream connected oscillator evaluates the coupling of both coils.
New Inclination Sensor F99 from Pepperl+Fuchs An all position sensor
The new F99 inclination sensor from Pepperl + Fuchs combines durability and simplicity into one small housing, making it ideal for industrial environments. The F99 inclination sensor provides a standardized 4 … 20 mA analog interface with a selectable angle measurement range between 0 … 360° without the need for a costly bus system. A spring mass system enables fast response times, Pepperl+Fuchs offers these non contact sensors in both, single- and dual-axis versions. Using two Teach-In buttons you can easily adjust the switching outputs.
RFID handhelds for 125 kHz, 250 kHz and 13.56 MHz Mobile RFID readers HH20 – ideal for logistics
Mobile reading of RFID tags has now been improved with the new generation of HH20 handhelds. The devices in cell phone format have a graphical display, direct control with variable menu buttons, and permit client-specific program sequences.
Block control system for electric overhead conveyor rails NDN20 for increased flexibility in the automotive industry
Electric overhead conveyor rails (EHB) represent one of the most important conveyor systems in the automobile industry. Within the automotive plant, overhead conveyors support the flow of materials from basic structure to final automotive assembly. A large number of complicated procedures have to be integrated perfectly, requiring impressive concepts and control technology.
Pepperl+Fuchs GmbH, Mannheim Geschaeftsfuehrer/Managing Directors: Dr.-Ing. Gunther Kegel (Vors./CEO), Dr.-Ing. Peter Adolphs, Werner Guthier, Mehmet Hatiboglu Vorsitzender des Aufsichtsrats/Chairman of the supervisory board: Dr. Volker Langbein Registergericht/Register Court: AG Mannheim HRB 4713