Druckseite anzeigen.
About the movies

305
Serviceline Factory Automation

Phone +49 (0)621 776-4411
fa-info@de.pepperl-fuchs.com

Inductive sensors for component detection in automobile assembly

In the finishing of blank parts in automotive and general engineering the presence of components is ensured by means of inductive sensors. In this special case, it is an inductive sensor with reduction factor 1. Irrespective of the materials used (steel, copper, aluminum, ...), the operating distance always remains the same. Another highlight of the sensors used for this application is the electrical and mechanical resistance to external welding fields. Thus, these sensors are especially suitable for use in welding robots.

back




Right click on this link, and choose "save target as..." to save this movie to your computer.



Pepperl+Fuchs GmbH · Lilienthalstr. 200 · 68307 Mannheim
Tel. 0621 776-1111 (Factory Automation)