»C-Series« is Coming and It's Looking Good
The new C-Series of the K-System was presented to the specialist public for the first time at this year’s Interkama. The positive reaction to this new variant within the K-System has shown us that we have once again scored a hit that takes us one step ahead of the rest of the field.
A great space saver: the C-series.
The new c-series brings a wider range of functions into the market. Prices for the series are identical to their functional counterparts in the F-Series. Approvals like ATEX, IECEX are already available. We are working on other approvals, like cFMus, which should be available shortly.
C-Series Overview
| Device variant | Description | Special features |
| KCD2-SR-EX1.LB | Isolating switch amplifier, 1-channel | 2 Relay outputs |
| KCD2-SR-EX2 | Isolating switch amplifier, 2-channel | 6.2 mm per channel |
| KCD2-STC-EX1 | Transmitter supply device, Isolating transformer | HART, 3-conductor input |
| KCD2-SCD-EX1 | Isolating transformer | HART |
| KCD0-SD-Ex1.1245 | Valve control module | Loop-supplied |
Availability
Series production of the first four devices in the table above is now underway, we will start delivering devices in August.
Protecting Your Process