The great migration – Field bus integrates Ex-protection, SIL and analog signals
The field bus is being used ever more frequently in process automation. Restrictions due to the requirements of explosion protection are no longer a theme and the new protocols for safety-aligned field bus applications are resulting in parallel-wired analog safety systems becoming superfluous. So no problem for new plants on green field sites. But what about the many existing plants with analogue signal transmission? Here the integration of remote I/O technology in the field bus offers an ideal platform for migration and plant extensions.
Pepperl+Fuchs Fieldbus Technology
"Field bus technology has proved to be extremely helpful in keeping to the tight schedule for the construction of the Clariant ruby plant" [1].
"The main problems of the new field bus technology have been solved; proven solutions are now installed at Novartis" [2].
"Future projects by Aventis at Höchst will be achieved using field bus technology" [3].
Clearly, these three notable users of process automation technology, and in the meantime many others [4], are convinced of the advantages of modern through going digital data transfer from the field devices to the control system using PROFIBUS PA and FOUNDATION Fieldbus H1. In the past, solutions have had to be found for several areas of doubt, which were formulated in the 2002 FuRIOS Study [5]. But now, in 2007, we have the answers to:
- Inadequate power in the field due to explosion protection through energy limitation
- Lack of incorporation of safety-aligned signals
- New, complex requirements for planning and maintenance
- Inadequate availability due to a lack of redundancy
- Incomplete incorporation of existing conventional field devices
High Power Trunk Concept – the end of the power shortage
Explosion protection through intrinsic safety limits the energy in the signal circuit in such a way, that no explosion-causing sparks can be generated. That which presents no problem in a conventional loop with a field device, a cable and an Ex i barrier, is simply impossible in the field bus network with up to 31 devices and a cable length of 1900 m. The solution was presented at NAMUR in November 2004 [2]: Field bus barriers. These distributors provide an intrinsically safe connection for each field device, which in addition is individually protected from short-circuiting. The connection between the barriers, the so-called trunk, is designed to provide increased safety (Ex e), which enables the injection of high energy in Zone 1 (Figure 1). Corresponding high power trunk concepts for Zone 2 are also possible through segment protectors with connections in Ex nL (in future Ex ic) [6].
High Power Trunk Topology, also for SIL applications
Safety-aligned field buses – doing away with parallelism
On all previously constructed plants conventional wiring for safety purposes has had to be installed parallel with the field bus network. This will not be the case in the future. For PA and H1 protocols have been developed up to SIL 3 [7], based on NAMUR Recommendation NE 97. The user tests are running, soon process and safety signals will be transferred in perfect harmony via a common field bus cable. And the good news is: The installation technology is not subject to any SIL consideration!
Planning and maintenance – drag & drop with online diagnosis
It was often feared: Planning and maintenance changes significantly with the field bus. This is true – both are significantly simpler! The layout of a field bus segment can take place virtually on a PC, including the automatic calculation of the energy balance, simulation of fault cases and the generation of equipment lists. Software design tools, such as the Segment Checker, which is available, free of charge on the Internet (www.segmentchecker.com) offer extensive device libraries, from which the segment can be assembled with a few mouse clicks.
And the indispensable multimeter for maintenance work? It is replaced by so-called Advanced Diagnostic Modules, which monitor the field bus installation on-line, immediately signal set value deviations and potential fault sources to the control room and even record the minimal ageing processes in the wiring [8]. Even the regular preventive removal and examination of field devices will become a thing of the past thanks to the evaluation of the diagnostic data available via the field bus.
High availability required – the answer is redundancy
In 2004 redundant field bus components [2] were called for at the NAMUR main assembly. Today they are available: PLC with redundant field bus cards, power supplies, such as the FieldConnex® Power Hub with modular replaceable, redundant power modules [6, 8]; the first systems with trunks aligned parallel in the field were presented at the Interkama exhibition 2006.
FieldBarriers and Fieldbus Process Interfaces
in major industrial use
Analog signals – no problem with field bus process interfaces
In existing process plants there are millions of analog and binary field devices in use, which, understandably, one doesn't want to lose. This led to the development of field bus process interfaces, which bundle the signals from many sensors and actuators into a single field bus message and thus integrate them efficiently into the digital communication (Figure 2). So, for example, the FieldConnex® Temperature Multi-Input incorporates the values form eight temperature sensors. On modern field bus remote I/O Systems, like the LB/FB Series, almost all analog field devices can be connected. The modular construction of these systems enables optimum matching to any process plant. Migration strategies can be developed for the successive modernization of existing plant in conventional technology towards full field bus communication [9].
Literature
- [1] Eichhorn, T., Pelz, M.: Fit for the future – Field bus technology at Clariant, in: CHEManager 07/05
- [2] Zobel, J.: Field bus at Novartis, in: Schwibach, M., Meier-Künzig, T., Seintsch, S., Zobel, J.: Field bus, reports on experience, Presentation at the NAMUR main assembly 4th November 2004, in: FuRIOS 2 Compendium, Pepperl+Fuchs GmbH, March 2005
- [3] Seintsch, S.: Summary of the Aventis Ketek plant, in [2] see also: Eckert, C.: The field bus grows up, MessTec & Automation 12/2004
- [4] see: Field bus installations at www.fieldbus.org and www.profibus.com
- [5] Tauchnitz, T., Schmieder, W., Seintsch, S.: FuRIOS: Field bus and Remote I/O – a system comparison, atp Automatisierungstechnische Praxis 44 (2002), issue 12
- [6] Kasten, T., Schüssler, B.: Breakthrough in field bus technology – High Power Trunk concepts, atp Automatisierungstechnische Praxis 45 (2005), Vol. 7, pages 47-53 available as reprint 187241 from Pepperl+Fuchs GmbH
- [7] Hug, U., Kasten, T.: Installation technology for safety – Field buses, presentation at the PCIC Petroleum and Chemical Industry Conference Europe, Basle, Switzerland 26th – 28th October 2005; appeared as extended reprint 198386 at Pepperl+Fuchs GmbH, December 2006
- [8] Hennecke, A.: The call for higher availability – Redundancy and Diagnosis PROFIBUS PA Networks security, in: P&A Compendium 2006/2007 see also: Kitchener, R.; Rogoll, G.: Advanced Online Physical Layer Diagnostics, Technical White Paper 198641 from Pepperl+Fuchs GmbH, August 2006
- [9] Hillebrand, R.: Incorporation of Remote I/O in control systems, Application reports – Pepperl+Fuchs GmbH, November 2006