DeutschEnglish homecontactfactory automationprocess automationproductsthe companyjobs und careers

Product Search:
Text Search:
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
    Safe data transmission, long distances: Fiber Optic Link for Profibus Communications

    In the chemical, petro-chemical and pharmaceutical industries as well as in the oil and gas sector explosion hazards must be avoided by suitable means at all times. For this purpose measurement and control installations rely on Remote I/O more and more. These employ PROFIBUS which makes use of fiber optic links to bridge long distances at high speed.

    Reliable, Economical Operation

    Plants stretching over a wide area often employ redundancy in their control system because of the high economic importance to maintain production. Since high speed PROFIBUS only permits the use of copper cable for short distances fiber optic links (FOL) offer an ideal alternative.

    There are three main differences with copper cables which make FOL the right choice in process control applications.

    • First fiber optic links ensure full galvanic isolation between the plant area and the control room.
    • Second the low energy levels of light cannot generate sparks or hot surfaces.
    • Third electro magnetic fields cannot cause interference in the fibers unlike in data transmission via copper cables.
    New Zone 1 Fiber Optic Link in GRP enclosure

    New Zone 1 Fiber Optic Link in GRP enclosure


    Furthermore the FOL Profibus-Repeater presented here offers some additional features. It can be used in a point to point application as well as in a redundant ring. It is capable of detecting Profibus faults and can induce a redundancy line change automatically. At the Zone 1 plant level of the Remote I/O station conventional bus cables are used. As the RS485 link is not intrinsically safe the cable must be wired in a similar way to power cables as to satisfy increased safety requirements.

    Summary

    Fiber optic technologies are the key to bus systems extending into the hazardous area. This enables improved efficiencies achieved in other branches of automation to be transferred to process automation without restriction. Fiber optic installations will continue to rise significantly especially as investments are being undertaken to extend the plant life by modernizing control systems.

    Our Products

    Additional Information