Digital Kanban Management
The software developed by Neoception provides the central logic for reading and aggregating local sensor data. Using smart pattern recognition, the software determines whether, when, and how a box movement occurred on the different tracks of the Kanban rack. Shorter, unintentional activations are carefully filtered and ignored. The higher-level Nexeed Industrial Application System from Bosch Connected Industry is informed only when clear-cut events have been identified. The Kanban service controls the RFID read heads and the LEDs.
In addition to operational functionalities, the service includes an online interface for simple hardware setup, operation monitoring, and debugging. Updates are quick, secure, and can be implemented via direct access to the main controller. Continuous checks on the functionality of all components enables comprehensive condition monitoring, the results of which are visualized as operating states via the stack light.
When it comes to providing in-depth information, the digital Kanban management system is far superior to conventional solutions: Each rack is fitted with a component kit comprising a photoelectric light strip, a dedicated rack controller, and an LED module for visualizing the put-to-light instructions.
Individual visual background suppressors are fitted to the specially developed sensor bar, which is available in different lengths. The background suppressors detect patterns in the software almost in real time. These patterns make it possible to draw conclusions about the movements in the racks. Based on this information, the LED module uses colored signals to indicate to the operator whether or not the box has been placed on the correct track.
The familiar AS-Interface flat cable with piercing technology enables operators to connect the racks quickly and flexibly.
简要介绍两家公司如何将定制化的工业传感器和物联网软件结合在一起,率先开发出市场上实现看板机架端到端数字化的解决方案。
在这段视频中,Neoception 产品负责人 Tobias Kehl 介绍了他与 Neoception、博世互联工业和倍加福合作开发的“智能超市”数字化看板管理系统。
在关于数字看板管理的小组讨论中,Sebastian Pesch、Stefan Schumacher(博世互联工业)、Bernd Fischer 和 Fabian Ritter(Neoception GmbH)与您共同探讨了关于“智能超市”的项目见解。
How have Kanban systems developed over the years? What weaknesses do they still suffer from today? How does the digital Kanban management system differ from conventional systems? Pepperl+Fuchs magazine "amplify" answers these questions.
Would you like to receive additional, in-depth information about digitalizing Kanban systems? Tobias Kehl, Digitalization Engineer at Neoception, has written an exclusive whitepaper on this subject. This PDF document explains basic Kanban workflows, highlights optimization potential, and explores the topic of cloud integration and the associated security considerations.
Visual overviews of process sequences, hardware components, and software architectures provide a quick way to understand how all of these elements are connected.
Get your free download now!